I need suggested parts to make:
Pro Class G audio amplifier power supply
Class G with modulated power rails, 15 volts absolute beyond channel output
Outer rails +/- 100 Volts, 20% ripple with full load
Inner rails +/- 50 Volts, 20% ripple with full load
When normalized loudspeaker peak power is 5000 Watts, average power would be about 250 Watts over 8 music bar-beats. I was after both positive and negative power factor controller IC’s to make the above power supply. I also want to control the initial switch on in-rush current to the capacitor banks, three seconds to charge up capacitors in the power supply.
I was considering using 2 x 50Hz 500 Watt isolation toroidal transformers to make the power rails.
I don't want to use any electro-mechanical relay's if possible.