This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3846: Duty ratio of PWM to UC3846

Part Number: UC3846

Hi engineers,

I use UC3846 to implement push-pull application, the present question is that Vin1 powered down, pin11 and pin14 duty ratio is 40%;  Vin powered on, the duty ratio is very small, only about 5%, above the two situations the duty ratio can not be adjustable. Please help to give some support, the schematic as illustrated.

Thank you very much!

Best Regards,

Jenny