This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are using UCC28063 + UCC256303 for a 500 W AC/DC project. We are now working on bring up the UCC256303 and see a symptom that Ho pin of UCC256303 no output waveform shown below. Any suggestion where should we check on UCC256303 circuit ? thanks!
Hi PYTsai,
Thanks for your interest in UCC256303. I would suggest making sure the boot cap is getting sufficient charge to supply HO. Also check the VCR waveform and make sure the common mode voltage is close to ~3V. Are you testing under any load? If you can share your schematic, I can take a look to see if everything looks ok.
Best Regards,
Ben Lough