This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm currently debugging a prototype of the UCC28740 + UCC24636.
5V - 2,5A
After one obvious correction around transformer primary (wrong polarisation) I get an unstable 5V on output. And the circuit cannot bear any load.
It seems that the UCC28740 was working properly on few switch, achieved to get a 5V but suffers a default and switch OFF.
We can see VDD drop below UVLO 7V
I was starting to investigate further with 2 differential probes but I burn a 2nd PCB (Rcs resistors). (on First PCB Rls, Rcs and UCC28740 burnt)
I got a differential probe between primary GND and VDD and the second one between primary GND and DRV.
Could the probe on the DRV triggers the Mosfet and build a short circuit on Rcs resistors?
Could you make a sanity check of my schematic before I go further on my live testing attempts?
Thank you
Best regards,
Frans
Dear Kevin,
First screen was Vaux yes. I include another one in my following informations.
Second screen was on Vdd capacitor yes.
I’ve already tried to increase C10 capacity (+10uF) but it only increases the time where switcher is inactive, my thought:
Now I think the UVLO is not the problem.
From my previous observation on scope, I could see the switcher (UCC) active during 3ms, then no more activity during 300-500ms that should deactivate the UCC which restart again from HV power.
I made test on 100, 300 mA and empty loads.
Here is output with empty load
Here is with 100 or 300mA load (bench electronic charge):
500ms period, 60ms between beginning of rising and return to 0V
We can see here the 3ms activity on the output
Here is activity detail during 3ms(measured on Vds of the Sync Rectifier UCC24636 on 100mA charge) happening every 500ms
With a frequency looking correct.
I’ve tested the slua783 2.6.2 Transformer saturation on Vcs: seems no problem
And last observation I was able to get before 2nd board burn:
3ms activity seen on Vaux
+30/-30V +18V without ringing.
Kevin, I’m satisfied by the way you’re exchanging with me and hope we can investigate further.
I’m a beginner on live line power supply (more used of DSP, MCU…) so I’m a little bit nervous testing this stuff.
I would really like to get possible correction before testing and getting it burn again (note previous card was tested multiple hours with very short test run before flashing).
Thank you,
Best regards,
Sorry after modification (on SR Vcs branch) and short test I still have unstable output.
Switcher is still pulsing during around 3ms and restart activity after ~600ms.
And we can see switcher going in protection after the 3ms and the Vdd depleting till 7V and switcher restart.
Output under 100mA load:
And output + switcher Vdd(blue):
I feart to push test more longer as it seems last correction doesn't solve the main problem and I fear to destroy this 3rd board.
Have you any advice on what to test/measure in priority? (I will have on more look on the SLUA783 Troubleshooting TI PSR Controllers, to find also by myself)
Thank you for your attention.
Best regards,
Hello Ulrich!
Sorry I saw your answer only one week after you post it (did miss the notification mail I think)
Thank you for your detailed explaination, it is very instructive.
So for my feeling about VDD I'm more and more confident that VDD is an effect and not a cause.
The cause seems to be the VS OVP like you pointed it.
First I tried to correct 2 things, put the full bank of output capacitors, thingking that the not enought capacitance could drive to a too fast rise of the output and cause the overvoltage. So I added the second 1500uF as described in the schematic (C1, C2)
But no change.
Then I corrected D3, as the chosen diode specs wasn't strong enough in front of the calculated values in SLUC487b sheet.
Replaced by a 1N4448WS that could handle the 250mA 67V (BAT48J 200mA weren't enought).
But no change on result.
Before putting your advised modification on Rvs2, I made measurement on VFB as I get some doubt about.
VFB in yellow, Vout on blue
Vfb seems too high for me. as it is described to have full range between 0,75-1V
So finally get your modification on Rvs2.
Used a 220k on // of 23.7k - Should get, from Ti calc sheet, an OVP value moved from 5,457 to 5,840V
The load is still on 100mA
Does the ~20 pulses used to charge the SR (UCC24636)?
Switch seems to have correctly started. But the output ripple seems really high for such low load. 900mV (100mA)
And Vfb seems really high also at 2,54V
Output after 1s.
Of maybe that's my bench electronic load that is involving ripple on the output.
Will be glad to get your advice before continuing torturing this PCB.
I will check and get some learning from the Debug PSR slua783 for the high ripple output issue.
Best regards,
Frans.
It's good to hear that.
You are always welcome to reach us out here
Best Regards
Kevin