This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610: BQ24610 query

Part Number: BQ24610
Other Parts Discussed in Thread: BQ24600

hi,

i look up bq24610 datasheet.below query need to be resolved,please help.

1.if my system power supply get from battery directly,our bq24610 can run normally?in this case,there will be no BATFET;then,vcc is only get power supply from  adapter,therefore,when the circuit is not in charging status,that is to say,no adapter plug in,vcc will no power supply,our bq24610 will be power off,our circuit also run normally?

2.if we refer to typical application circuit, BATFET will be aways on, that is to say,our system can directly get power supply from battery , do we need operate BATDRV pin to turn on the BATFET?even if  we turn off the BATFET,the system also can get power from battery.why we also need the BATFET.

3.can you provide   a lowest cost application circuit about bq24610 for me?such  as taking out two ACFET or BATFET;

thank for you support.

best regards.

Cickey xu.