This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM84624: Can I place more than one TPSM84624 in parallel, to share current (i.e. ORing)

Part Number: TPSM84624
Other Parts Discussed in Thread: LMZ31710

  I would like to use several TPSM84624 in parallel to increase (multiply) the current output.  I'm willing to use any number of passives and/or feed-back circuits, etc...  To make this happen... 

  I'm looking to create a 1 ~ 8 Volts variable supply at 40 Amps.  Any ideas?  FYI, the output voltage will vary, and will drive a load which is almost entirely resistive.

  I could try the classic diode ORing, or better yet, use a MOSFET configured to operate like an active diode (similar to synchronous rectification circuit).

  I will also consider placing other TI SMPS circuits in parallel if someone can recommend a good target for this.