This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Input voltage range is 9V~36V, normally working at 12V or 24V.
Output is 19.5V/1A.
Please help to confirm schematic and component parameters.
Is it necessary to modify?
Thank you
Jerry
Hi Jerry,
From my initial review, R8 should be 0 Ohm to begin with and raising it in EMI testing if needed. R8 gate resistance of 100 Ohm is also quite high.
You also do not need R4 or VR1 since this is taken care of the the PDRV of the TSPS92692 already. With DIM/PWM input is being pulled high you will not need to have R13 unless you are PWM'ing.
4.7nF (C24) seems to be high for a snubber and I would recommend using 470pF to begin with.
What is the part number for L3 or saturation current of L3?
Thanks Tuan