This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92692: Confirm schematic

Part Number: TPS92692

Hi

Input voltage range is 9V~36V, normally working at 12V or 24V.           

Output  is 19.5V/1A.      

Please help to confirm schematic and component parameters.           

Is it necessary to modify?

Thank you

Jerry