Hi,
I'm using PTH04T241WAS as my MPC8548 PowerPC CPU core power supply. The input is 3.3V, and the output is 1.1V.
In the operation, when the output 1.1V ramps to 0.4V, we can find inrush current happens on the 3.3V rail. And this inrush current is far higher than all I/O current, most importantly, it causes the 3.3V drop. This is harmful for other devices connected with 3.3V power plane. The inrush last time is about 800uS.
We changed the soft start capacitor's value to 10nF on the module(which connects with TPS40100's SS pin), the inrush last time decreased, and it also happened when 1.1V output ramped to 0.4V. Futhermore, we found that if the 3.3V doesn't finish discharging, and then we powerup again, the inrush will dissappear!
In our application, the tracking function is disabled by connecting the TRACK pin directly with Vin(3.3V), and sense function is also disabled.
In our system, because there is only one 3.3V rail input, that means we power up the I/O supply prior to core supply, and this is allowed by MPC8548 spec.
My questions are:
1. Is it possible that this issue is caused by pre-bias start-up?
2. What other factors can cause this issue?
Need experts here help to take a look at this issue, thanks a lot in advance.