This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO5452: What is the value of internal Pull-down resistor and pull-up resistor?

Part Number: ISO5452


Hi team,

         As we known, in ISO5452, there are internal Pull-down resistor in IN+ pin and internal pull-up resistor in IN- pin.

        What is the resistors’ value of  internal Pull-down resistor and pull-up resistor? We can’t find in the datasheet.

Do we need add external resistor between IN+ pin and IN- pin? Because there are internal Pull-down and pull-up resistors, I think it don't need add external resistor between IN+ pin and IN- pin. But why do some boards still need add it ?

Could you have any idea and suggestions?  Thank for your help! 

  • Hi Eggsy,

    The value of internal pull-up and pull-down resistors is between 40k and 100k across PVT corners.

    With Regards,
    Xiong
  • Hi Xiong,

              Customers tested the the internal pull-up and pull-down resistor value and the value is about 400K.

    May I know if something is wrong? Testing way or others?

    BTW, as you said, the internal pull-up and pull-down resistor value is between 40k and 100k across PVT corners. Why the values is so wide different? Will it cause some problem?

    Thanks!

  • Hi Eggsy,

    You can add a pull-down resistor on the IN- and a pull-up resistor on the IN+. Those resistors would form voltage dividers with internal pull-up and pull-down resistors. You can measure the voltage on the IN+ and IN- pins. Please not actively drive those pins during the tests.

    The internal pull-up and pull-down resistors are intended to be used to position IN+ and IN- pins to defined states. The value does not need to be very accurate. It is common for on-chip resistors to have that wide range.   

    With Regards,

    Xiong