This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear ti,
I have read the slua585 design resources,there is a description of a paragraph in the below
in the slua585.pdf .
For stand-alone charger, it not only has a LC resonant range, but also has Cmax_wake or Cmax_dis
calculation which is derived from the battery detection parameter [see bq24610 data sheet (SLUS892)]. If
the output capacitor is over Cmax, the status pin will flash even when battery is absent.
Also, if the resistance is too high between charger output and battery terminal, the charger will run in and
out of charger termination.
Rbat_max = Vrch/Iterm
Vrch: Recharge threshold voltage; mV/Cell
Iterm: Termination current.
the Rbat_max is the battery internal resistance ? or the resistancecharger output and battery terminal ? or The sum of the two ?