This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a 5V rail and want to charge a 2.7V supercapacitor. It looks reasonable to use the LM2665 to generate 2.5V (Vin/2) and use that to charge the capacitor. My question is whether I can rely on the 40mA max current of the LM2665 to operate as constant-current charger, or whether that will potentially harm the device. The discharged supercap will basically look like a short circuit so I worry that this won't work. I could put a 62Ω resistor in series with the supercap, thus limiting the max current to 40mA, but as the capacitor voltage rises the charging current will decrease, significantly stretching out charging time.
Any advice on this, either for a way to use the LM2665 or some other circuit I am overlooking, is appreciated!
The capacitance would be somewhere between 1.5F and 6F. That would look like a short circuit for a lot longer than 1 sec...
The input voltage is a fairly well-regulated 5V, so I'd feel comfortable saying it would never go over 5.4V, and Vin/2 would never go over 2.7V.
I wouldn't want to limit the current to something as low as 8mA. Even 40mA is less than I'd really want, but it's the highest Iout I found in a charge pump of this size.