This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCV010505D: Output power is lower than expected

Part Number: DCV010505D
Other Parts Discussed in Thread: DCV010505

Hi,

I made a circuit that uses DCV010505D to get isolated -/+5v output from +5V USB power. When I soldered everything and tested, I found the output was about -/+2V at no load. I don't have the 2.2uF capacitor at the current moment so I paralleled two 1uF ceramic capacitors for the input pin. I don't know if the issue is the wrong capacitor or others. I'm going to buy the 2.2uF capacitor and try it again. But I read that someone has a similar issue from this thread and I wonder whether they have resolved their issue or not. Look forward to your reply, thank in advance.

Thanks

Rui