Other Parts Discussed in Thread: UCC28070, UCC28180
I am trying to construct a power factor correction scheme for a 3 phase 400Vac power supply.
According to previous information from TI, boost topology is suitable for industrial enviroment so that I eliminated the buck topology which may have some other advantages.
I selected UCC28070 as the controller. (boost topology)
I do not want to use the neutral line, The power supply has to use only the 3 phases.
What can be the best arrangement for this setup?
I send the following schematics containing 3 seperate PFC units for each phase.
Each input is between phases. This setup does not need neutral point.
Would you recommend a simpler setup containing less switches and diodes. This setup needs 3 HV igbts and 3 HV diodes.