Other Parts Discussed in Thread: UCC24636, , BQ24650
Good day
Hope someone can assist me with the problem.
I have read similar posts on the same issue, the device does not startup.
Currently I only get one pulse every 1.2 seconds.
Attached is my schematic. Note that during the testing I have changed the following.
R13 = 300mR
Added 180pF cap on CS pin
C7 = 10uF 50V Ceramic
L1 was removed for testing and shorted. The signals did not change after this change.
On Images DS0001.bmp - DS0005.bmp the signals are:
1) Yellow - DRV measured on Mosfet Gate - Max voltage = 5V @ 10us
2) Blue - Vdd measured on pin 1 - Max voltage 20.8V
3) Pink - CS pin - measured on pin
4) Green - VS pin - Measured on Pin
On DS0006.bmp the green is FB pin
On DS0007 Green is the Aux coil output before R14
D1 is a Bidirectional Protection Diode - SMBJ110C, Will this cause the problem? I had this in stock. The unidirectional one is SMBJ110A.
DS0001
DS0002
DS0003
DS0004
DS0005
DS006
DS0007
Schematic