Other Parts Discussed in Thread: BQMTESTER, EV2400, BQPRODUCTION, BQ34Z100, BQ34Z100-G1, BQ34110, BQ40Z50, BQSTUDIO
Hello,
I am using the bq40z50-R1, configured with bq studio.
Now I would like to test it with the production tool bqMtester ( HPA495 rev A) + EV2400
I followed the schematic SLUU397A–figure 2
I can't communicate with bq production SBB, the led "current on" and "voltage on" stay OFF on the bqMtester.
It seems J1 vout should be 5V to work properly but it is 0V? does the EV2400 supply the I2c or do I have to add a second external 5V?
Thanks,
Clement