Dear Sir,
I would like to set up the temperature 0~45 degree C. May suggest me the thermistor valute ?
also, does BQ24079 have output over-voltage protection from battery side, like (4.2v battery )? thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
I would like to set up the temperature 0~45 degree C. May suggest me the thermistor valute ?
also, does BQ24079 have output over-voltage protection from battery side, like (4.2v battery )? thanks.
Hi Lucifer,
We have a Linear charge NTC calculator that can help you with calculations set up temperatures. The BQ24079T has voltage based TS monitoring iif there is no suitable resistor values on the BQ24079. As for OVP on the battery side, normally a PCM module is used on the battery end to protect from over voltage.
Anthony P Pham said:Hi Lucifer,
We have a Linear charge NTC calculator that can help you with calculations set up temperatures. The BQ24079T has voltage based TS monitoring iif there is no suitable resistor values on the BQ24079. As for OVP on the battery side, normally a PCM module is used on the battery end to protect from over voltage.
Hi,
Did this help in answering your question?