Hi,
I'm testing the TPS2543EVM evaluation board and set it to CDP mode. I connect its output to a Lenovo 5" tablet and monitor the battery charging status. When I connect the input of this board to a 5V DC supply, my tablet shows charging over AC and I suppose the board is indeed in CDP mode with maximum 1.5A charging current. However, when I connect the input to a PC USB port, the tablet shows "charging over USB". I think the board is no more in CDP mode and the maximum current is only 500 mA.
So my question is besides the control pins what else can make the board out of the CDP mode? (into SDP mode?)