Other Parts Discussed in Thread: BQSTUDIO, , BQ24161
Hi everyone,
I've tried to set the charge current limits basing on the battery temperature using Charge Current Tn parameters of the Fuel Gauge registers, but it seems like their values don't limit the charge current at all. I've played with different values, even tried to limit the charge current to 5% of the designed capacity value for all temeperature ranges. The only value of Charge Current Tn parameters that seems to affect the charge current is 0 because at this value the charge current drops to 0A.
How do I make this system to actually limit the charge current basing on these Charge Current Tn parameters?
Regards,
Pavels
P.S. I'm using bqstudio 1.3.86 for changing these paramers and to see the measured battery charge current. The system consists of BQ27530-G1 that controls BQ24161 battery charger. Golden Image file is attached to this message.