This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM1085: negative output voltage

Part Number: LM1085
Other Parts Discussed in Thread: TPS54302, LM337

We plan to use LM1085-ADJ to generate +7.5V and -7.5V from 12VDC input. Can we use this to generate neg output voltage? If so any ckt using LM1085-ADJ,

Attached a schematic for +7,5V out with 12VDC in

This is for a analog board so like to keep it Linear than switched buck (TPS54302)mt_power_LDO_RevA1.pdf