I measured the voltages at each node and compiled them into a document.
The post is locked on E2E, I couldn't reply directly, so I'll send you the material here.
Please check it out.
When the noise is audible, it is at least taper-charged, but the conditions under which the noise is audible are more complex and less reproducible.
I thought that audible noise also occurs when there is oscillation in the VSW as shown in fig.2B and fig.3B, but this does not seem to be the case.
The audible noise was also generated when there was no oscillation in the VSW as shown in fig.4.
The oscillation of VSW is probably due to the parasitic capacitance of the inductor, which is a behavior specific to DCM step-up converters, and the schematic of the BQ25887 evaluation board (SLUUC12) shows that a snubber circuit can be mounted on the SW pin, which may be a solution to this problem. It seems to be the case.
Since the mounting area is small and there is no microphone for measurement, I can't determine which component is emitting the sound, but it could be C19 or L1 in the schematic.
Can you suggest a hardware or software solution?
Sorry for the long wait for your reply.