There was a problem using LM25122-Q1.
Input : typ 12V
output : 24V, 2A
However, the customer has a shutdown in output load 1.8A.
Could you review my schematic as attached file.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There was a problem using LM25122-Q1.
Input : typ 12V
output : 24V, 2A
However, the customer has a shutdown in output load 1.8A.
Could you review my schematic as attached file.
Hi Brigitte
Sorry for the late reply.
The customer checked late because he was on vacation.
1.Attached is the inductor specification.
2. The inductor current measurement is not confirmed.
However, the customer tested the inductor change, and the problem was not solved..
Inductor Part : EMA13050S-330M --> EMA13050S-100M
Hello CHO,
Changing the inductor from 33uF to 10uF will not really help to increase the current, as this increases the ripple current by a factor of 3.
What is the minimum and maximum input voltage? Could you please ask the customer to check the input voltage on the input capacitor at 1.8A output current?
Hello CHO,
The current rating of the inductor seems not to be sufficient for the application. Please exchange the inductor with at least 11A current rating and check the maximum output current again. (this is only for testing)
Hi Brigitte
Hi Brigitte
Please test with a 33uH inductor with 11A current rating not a 10uH with 12.5A rating.
--> To be updated after purchase of inductor. ( ~ Aug 21 )
Please measure the voltage on the input pin while the output current is at the maximum achievable.
1. LM25122 Loadless EN pin input and output waveform.
2. Start after connecting load.(1.9A)
3. Shutdown after load connection. (1.95A)
4. After the shutdown.
5. No-load CSP & CSN
6. CSP & CSN After Load Connection
7. CSP & CSN during shutdown
8. Update the schematic to a pdf file.
Hello CHO,
As I did not hear back from you, I expect that you have been able to solve your issue and will now close the thread. If this is not the case, please post below or create a new thread if this one is already locked.