This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25122-Q1: LM25122-Q1 ISSUE & Schematic review

Part Number: LM25122-Q1

There was a problem using LM25122-Q1.

Input : typ 12V
output : 24V, 2A

However, the customer has a shutdown in output load 1.8A.

Could you review my schematic as attached file.

Schematic review.pdf