Dear colleague,
Our customer is using BQ27520-Q1, here is a strange issue.
This customer using the processor to communicate with BQ27520.
But when the processor restart, the processor can't communicate with BQ27520, and this BQ27520 looks like it's locked.
The customer checks the I2C waveform when the processor restarts, it is the same as normal operation. And other devices in I2C bus areormal.
When you do this, it will be 100% repeated.
So
1. Could you please give us some suggestions to debug?
2. What is the possible reason?
3. How to avid it?
Attached is the schematic.
6518.Charger circuit.pdf2768.Control circuit.pdf
Best Regards,
Rock Su