Hi Team,
My customer reported an issue that while the VDD drop and restored, the TPS40303 couldn’t provide normal output voltage.
The VDD provided by previous power module output which has the over current protection, if the load detected over setting which is less that TPS40303 OCP value, the VDD would pulled to less than 3V, and the PGOOD is pull to low. After the load removed, the VIN would be back to normal, but the output of TPS40303 couldn’t be restored.
Support Needs:
-
While the input restored, and output load is empty and couldn’t trigger OCP, From previous test waveform,
why the PGOOD signal could be restored?
- How to fix this issue?
The detailed description/schematic&PCB Layout/test waveform could be found as attached file.
Expect for your kindly reply.
TPS40303 Could be restore issue.docx
Best Regards
Benjamin