Hello -
I am having some problems with the LM5576 in a custom power supply. I have replicated the circuit from the LM5576EVAL board. The circuit works as expected with one setup, which has a nominal input voltage of 42V. However, in another setup, which has a nominal voltage of 54V, the IC is visibly getting damaged (spark/small flame, magic smoke). This has occurred over several boards (more than I'd care to admit) so it was not an aberration with one IC or board. Please help as this is causing us some pain at the moment!
Please find attached a circuit diagram as well as a photo of a burned-up IC in case this provides some insight.
Thanks very much in advance for any help/insight.
Best Regards,
Jamie Ahmed