Query: Q23 MOSFET has Part no ZXMP10A13FTA which has VGth -2.0V to -4.0 V & if the op-amp Vss current is greater than 2uA /4 uA then Q23 will turn ON & op-amp Vss will pull down to Cell0 (GND). In this case, Vcc at op-amp is Bus voltage which as per our design is 62 V for LFP Cell. In this condition, op-amp would fail.
Let me know your thoughts
With regards,
P.K.Jain