Hi, Team,
The customer has two questions:
- Is it ok to tie OUT0, OUT2, OUT6, OUT8 output pins to supply current to a single LED?
- When tying multiple outputs to supply current to a single LED, does it have to be either even or odd pin #?
*e.g., OUT1, OUT3, OUT5, OUT7 or OUT0, OUT2, OUT6, OUT8
The question is based on the figure 109 (page 57).
Could you please answer in yes/no for questions 1 and 2 separately with a reason if possible?
Thanks and Best Regards,
Masaru Oinaga