Other Parts Discussed in Thread: BQ25606,
Dear All,
I designed the single cell battery charger. My power source is 5V, 3A. I let the float VSET, ILIM = 205 Ohm (the input current limit is 2.5 A) and ICHG = 649 Ohm (the charge current limit is 1A). I monitor the SYS pin voltage is 4.2V with a maximum load of 470 mA. If I increase the load a little higher, the SYS pin voltage will decrease which means it could not handle the load greater than 470 mA. Based on its design, it should be higher. I don't know what goes wrong in my conception. I hope somebody can help highlight the problem.
Thanks