This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am testing UC3846 duty cycle at output with rotating potentiometer (by varying voltage) at EA pin EA(-). My maximum duty cycle is 38%. I am getting gradual change from 10% to 26% in duty cycle by rotating potentiometer at EA(-) pin. But after 26% it jumps to 38% directly. I changed the potentiometers & its values but the result is the same. Where is the mistake? Please help.
Thanks.
-Satyavijay
Thanks for support.
Between CS+ and CS- there are three resistors of value 0.16 ohm each. Voltage at pin1 is 0.5V. EA+ pin at 5.1V. I am testing with no load.
At present I have no scan copy of my schematic despite above information if needed it I will scan it and post.
Regards.