Other Parts Discussed in Thread: UCC2897A
Dear all,
Please help to check the schematic of attachment.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Vickers,
J2 RJ45 is not connected correctly. Note PoE power should come through Pair Set 1 of Pairs 1/2 and 3/6 then from Pair Set 2 of Pairs 4/5 and 7/8.
Bob smith caps C21/20/95/96 should be 10nF and not 100nF.
I see a diode bridge and hybrid bridge. Which one is customer using? The hybrid bridge does not look correct. I recommend copying the one on TPS2372-3EVM-757. If using the hybrid bridge I also recommend using the detection resistor that's recommend on the EVM I reference.
It is recommended to use TPH/TPL/BT signals as described below. But if your application does not need these signals then the connections are okay.
For the DCDC section, I recommend posting in the forums for the UCC2897A design. Thanks!