This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM335X: How to set Entry Point Address in SYSBIOS

Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: SYSBIOS, AM3359

Hello,

I think I asked they a few years ago, but now all my history was purged...  So here we go again.  Since it's been a few years, I have no idea where to start looking.

(I am using CCS 10, SYSBIOS 6.76, GCC Compiler... but I don't think that has any bearing on this)

The AM335x bootstraps from EMMC or SD into address 0x402f0400  That's fine.

The utility "tiimage.exe" will place a 4 byte size, and a 4 byte load address at the front of the binary (after it's been stripped down with arm-none-eabi-objcopy)

That's fine if you are NOT using a SYSBIOS project.

A little test SYSBIOS project I just build has an entry point that is NOT at 0x80000000  but c_int00 is located at 0x800040e0 (as I found out from the MAP file).   

Except the IMAGE has to load starting at address 0x80000000.

So, I can set the entry point using a conventional linker script, but the penchant to hide everything when using SYSBIOS means not only do I not know how to set the entry address, but I have to address these settings so rarely, that I forget...  because I don't deal with these concerns except every few years.

As far as I can tell, this isn't gonna work.  SYSBIOS placed the MMU table at address 0x8000000, and the "tiimage.exe" utility just ASSUMES that the start of the image is also the entry point.

Any suggestions, short of writing a CUSTOM BOOTLOADER every time there is a new SYSBIOS program that changes it's c_int00 address?

Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
ti.sysbios.family.arm.a8.mmuTableSection
0x80000000 0x4000
*(ti.sysbios.family.arm.a8.mmuTableSection)
ti.sysbios.family.arm.a8.mmuTableSection
0x80000000 0x4000 C:\...\Release\configPkg\package\cfg\app_pa8fg.oa8fg
0x80000000 ti_sysbios_family_arm_a8_Mmu_Module_State_0_tableBuf__A
xdc.meta 0x80004000 0xe0
*(xdc.meta)
xdc.meta 0x80004000 0xe0 C:\...\Release\configPkg\package\cfg\app_pa8fg.oa8fg
0x80004000 __TRDR__
0x80004028 __TARG__
0x8000404c __PLAT__
0x80004074 __ISA__
0x80004088 __ASM__
.c_int00 0x800040e0 0xb4
*(.c_int00)
.c_int00 0x800040e0 0xb4 C:\ti\bios_6_76_03_01\packages\gnu\targets\arm\rtsv7A\lib\boot.aa8fg(boot.oa8fg)
0x800040e0 _c_int00
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

-CSW

  • Hi,

    I'm not sure why your program had mmuTableSection at 0x8000000, but I tried an AM335x PDK example project, GPIO_LedBlink_iceAMIC110_armTestProject, and the .map file (attached) GPIO_LedBlink_iceAMIC110_armTestProject.mapshows the following:

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    .c_int00 0x80000000 0xb4
    *(.c_int00)
    .c_int00 0x80000000 0xb4 C:\ti\bios_6_76_03_01\packages\gnu\targets\arm\rtsv7A\lib\boot.aa8fg(boot.oa8fg)
    0x80000000 _c_int00
    ti.sysbios.family.arm.a8.mmuTableSection
    0x80018000 0x4000
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    You can compare your project with this PDK example project and find the difference. Please refer instructions here regarding how to create and build PDK example projects.

    Regards,

    Jianzhong

  • Jianzhong,

    That didn't take long to fail.

    Using CCS Import Projects, and navigating to the PDK folder,

    The PDK folder has only two examples in it.

  • You'll need to create the projects according to instructions at: https://software-dl.ti.com/processor-sdk-rtos/esd/docs/latest/rtos/index_overview.html#pdk-example-and-test-project-creation. Basically, you'll need to

    1. Install and register all SDK products in CCS.

    2. Create PDK example projects:

    • C:\ti\pdk_am335x_1_0_17\packages>pdksetupenv.bat
    • C:\ti\pdk_am335x_1_0_17\packages>pdkProjectCreate.bat AM335x

    Regards,

    Jianzhong

  • Jianzhong,

    Then CCS is not the preferred environment anymore?

    I have had exactly 0.0000% success using the batch files from these packages.  Apparently written by Linux shell developers who don't have any idea about Windows.

    Case in point below...

    C:\ti\pdk_am335x_1_0_17\packages>pdksetupenv.bat
    ***************************************************
    Environment Configuration:
    ***************************************************
    SDK_INSTALL_PATH : C:/ti
    PDK_INSTALL_PATH : C:/ti/pdk_am335x_1_0_17/packages
    GMAKE_INSTALL_PATH : C:/ti/xdctools_3_55_02_22_core
    PDK_SOC : am335x
    PDK_VERSION : 1_0_17
    RULES_MAKE : C:/ti/pdk_am335x_1_0_17/packages/ti/build/Rules.make
    ***************************************************

    C:\ti\pdk_am335x_1_0_17\packages>pdkProjectCreate.bat AM335x
    =========================================================================
    Configuration:
    SOC : AM335x
    BOARD : all
    ENDIAN : little
    MODULE : all
    PROJECT_TYPE : all
    PROCESSOR : arm
    PDK_SHORT_NAME : C:\ti\PDK_AM~2\packages\
    =========================================================================
    Checking Configuration...
    Complete
    =========================================================================
    PDK_PARTNO : AM335
    PDK_ECLIPSE_ID : com.ti.pdk.am335x
    RTSC_PLATFORM_NAME : ti.platforms.evmAM3359
    RTSC_TARGET : gnu.targets.arm.A8F
    CCS_DEVICE : "Cortex A.AM3359.ICE_AM3359"
    *****************************************************************************
    Detecting all projects in PDK and importing them in the workspace C:\ti\PDK_AM~2\packages\\MyExampleProjects
    Detected Test Project: EMAC_BasicExample_evmAM335x_armExampleproject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: EMAC_BasicExample_skAM335x_armExampleproject
    The system cannot find the path specified.Cancel
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: GPIO_LedBlink_bbbAM335x_armTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: GPIO_LedBlink_icev2AM335x_armTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    Detected Test Project: GPIO_LedBlink_skAM335x_armTestProject
    The system cannot find the path specified.
    Copying macro.ini
    The system cannot find the path specified.
    0 file(s) copied.
    .... 
    *****************************************************************************

    C:\ti\pdk_am335x_1_0_17\packages>

  • Those PDK scripts are just used to create the CCS projects. You'll still use CCS to build and debug after the projects are created.

  • I do NOT enjoy troubleshooting vendors 800+ line batch files...  Because they didn't test or document it properly...

    software-dl.ti.com/.../index_overview.html

    Quoting:

    Fullscreen
    1
    2
    3
    Ensure all dependent/prerequisite products are installed and registered
    with CCS before proceeding with the examples and/or unit test. Starting
    CCS after installing...
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    Okay...

    Fullscreen
    1
    Navigate to pdk_[soc]_[version]/packages
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    Okay

    Fullscreen
    1
    2
    3
    4
    5
    [Optional] Edit the product versions within the pdkProjectCreate script.
    The default settings in the pdkProjectCreate script will have the
    product versions installed with the PDK. The pdkProjectCreate script
    can be modified to use older or newer product versions based on the
    user’s development environment.
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    Not needed, I am using the same versions from the PDK installer.

    Fullscreen
    1
    2
    3
    If the CCS installation is located somewhere other than “C:\ti”, ensure
    that the pdkProjectCreate script has this location correctly specified
    by updating the CCS_INSTALL_PATH or set TOOLS_INSTALL_PATH variable
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    Well, it's not...  Everything is in C:\TI.

    And I still get all those errors.

    Well, guess what...?  Line 449 of the batch file is wrong.  My version of CCS is 10.1.1.   The batch files has 9.3.0.

    This instruction is ONLY telling the use to update if they didn't put the packages in the TI folder.  There is NOTHING about the version of CCS.


    Now can we get back to the original issue?

    The app I create with the wizard  (Project | New CCS Project | GNU SYSBIOS) places .c_int00 at address 0x800040e0

    The app I import places .c_int00 at address 0x80000000

    The ONLY difference is the contents of the CFG file, which is a bunch of JAVA adding superfluous packages I do not know what they are (finding doc on them is a nightmare) and I do not need or want.

    The REASON that .c_int00 is in the wrong place is because of the config/Pkg/linker.cmd.

    The one from the example:

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    15
    16
    17
    18
    19
    20
    21
    /*
    * This file was generated by linkcmd_bm_v7a.xdt from the gnu.target.arm package.
    */
    ENTRY(_c_int00)
    ...
    /* Content from ti.sysbios.family.arm (ti/sysbios/family/arm/linkcmd.xdt): */
    /* Content from ti.sysbios.family.arm.a8.intcps (ti/sysbios/family/arm/a8/intcps/linkcmd.xdt): */
    ti_sysbios_family_arm_a8_intcps_Hwi_intc = 0x48200000;
    SECTIONS {
    .c_int00 : {
    KEEP (*(.c_int00))
    } > REGION_TEXT
    .text : {
    CREATE_OBJECT_SYMBOLS
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    And the one from the wizard:

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    15
    16
    17
    18
    19
    20
    21
    /*
    * This file was generated by linkcmd_bm_v7a.xdt from the gnu.target.arm package.
    */
    ENTRY(_c_int00)
    ...
    /* Content from ti.sysbios.family.arm (ti/sysbios/family/arm/linkcmd.xdt): */
    /* Content from ti.sysbios.family.arm.a8.intcps (ti/sysbios/family/arm/a8/intcps/linkcmd.xdt): */
    ti_sysbios_family_arm_a8_intcps_Hwi_intc = 0x48200000;
    SECTIONS {
    .vecs : {*(.vecs)} AT> DDR2
    ti.sysbios.family.arm.a8.mmuTableSection (NOLOAD) : {*(ti.sysbios.family.arm.a8.mmuTableSection)} AT> DDR2
    xdc.meta (COPY) : {KEEP(*(xdc.meta))} AT> DDR2
    .c_int00 : {
    KEEP (*(.c_int00))
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    That file is MAGICALLY CREATED by this environment in a manner that is hidden from the user.

    Changing that file does no good because it is re-generated.

    Not only do I NOT enjoy troubleshooting other peoples batch files that are broken...\

    I do NOT enjoy troubleshooting environments where they try to obfuscate and hide ALL the controls, because they think they are doing you a favor. but not having to know what and where that stuff is.

    ...  and then berate you for not knowing how to modify/adjust//fix issues that are coming out of that same environment that was designed to make it not necessary for you to know how it works under the covers.

    Here is the ENTIRE project created by the wizard which places the .c_int00 in the wrong place.  Not a single line of code was changed from the original creation.

    EmptyTest.zip

    -CSW

  • Hi CSW,

    Jianzhong is on vacation and will be able to respond in the week of June 21. Please note delay in the response for this thread.

    Thanks

  • Great...  So nothing will happen for a week, short of me troubleshooting this obfuscated environment.

    So I continued to dig into your environment and here is what I found...

    The target device is a BeagleBoneBlack.

    This is an app created by CCS using the menu "Project | New CCS Project" and picking "SYS/BIOS | GNU Target Examples | Typical"

    I am including MY OWN interface functions, not the PDK libs. So all the GPIO calls are from source code within the project. Not linked in.

    I added a file CMD in the root to set the entry point to the start of DDR:

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    MEMORY
    {
    DDR : org = 0x80000000, len = 0x20000000
    }
    SECTIONS {
    .c_int00 : {
    KEEP (*(.c_int00))
    } > DDR
    }
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    At that point, the entry is set to 0x8000000

    But it is failing.

    I modified the bootloader to generate some diagnostic messages. I verified that the bootloader is working correctly.  it is.

    The bootloader will also load and run the Example GPIO_LedBlink_bbbAM335x_armTestProject  so I know the bootloader functions.

    I reset the device, and step through the bootloader execution from address 0x402F0400. The loader correctly loads the 'app' and executes a call to the target address of 0x80000000.

    Here it enters EITHER the sample program GPIO_LedBlink_bbbAM335x_armTestProject -OR- my program created with the Project | New CCS Project...

    The assembly at address 0x800000 is IDENTICAL between the two apps.

    However they jump to different locations at address 0x...98.

    On the EXAMPLE project imported:

    The instruction at address ...98 is BLX r0 and the content of R0 is 0x80000C04

    I can see this in the map file (xdc_runtime_Startup_reset), and it is one of those XDC generated source files:

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    .text.xdc_runtime_Startup_exec__I
    0x80000bd4 0x30 C:\ti\pdk_am335x_1_0_17\packages\MyExampleProjects\GPIO_LedBlink_bbbAM335x_armTestProject\Debug\configPkg\package\cfg\am335x_app_bbbam335x_pa8fg.oa8fg
    0x80000bd4 xdc_runtime_Startup_exec(int0_t)
    .text.xdc_runtime_Startup_reset__I
    0x80000c04 0x14 C:\ti\pdk_am335x_1_0_17\packages\MyExampleProjects\GPIO_LedBlink_bbbAM335x_armTestProject\Debug\configPkg\package\cfg\am335x_app_bbbam335x_pa8fg.oa8fg
    0x80000c04 xdc_runtime_Startup_reset(int0_t)
    .text.xdc_runtime_System_printfExtend__I
    0x80000c18 0x3c0 C:\ti\pdk_am335x_1_0_17\packages\MyExampleProjects\GPIO_LedBlink_bbbAM335x_armTestProject\Debug\configPkg\package\cfg\am335x_app_bbbam335x_pa8fg.oa8fg
    0x80000c18 xdc_runtime_System_printfExtend(int0_t)
    .text.xdc_runtime_SysMin_output__I
    0x80000fd8 0x84 C:\ti\pdk_am335x_1_0_17\packages\MyExampleProjects\GPIO_LedBlink_bbbAM335x_armTestProject\Debug\configPkg\package\cfg\am335x_app_bbbam335x_pa8fg.oa8fg
    0x80000fd8 xdc_runtime_SysMin_output(int0_t)
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX


    On the app generated by CCS, the same instruction at address is jumping to a different address. The contents of R0 is 0x80008EA8.

    When I look at the map file, that is not even an entry point. It is in the middle of my function GPIO2ModuleClkConfig

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    .text 0x80008ca4 0x224 ./ti/source/drivers/gpio.o
    0x80008ca4 GPIO1Pin23PinMuxSetup
    0x80008cb8 GPIO0ModuleClkConfig
    0x80008d9c GPIO1ModuleClkConfig
    0x80008e1c GPIO1PinMuxSetup
    0x80008e38 GpioPinMuxSetup
    0x80008e48 GPIO2ModuleClkConfig
    .text 0x80008ec8 0x584 ./ti/source/drivers/gpio_v2.o
    0x80008ec8 GPIOModuleReset
    0x80008ee4 GPIOModuleEnable
    0x80008ef4 GPIOModuleDisable
    0x80008f04 GPIODirModeSet
    0x80008f34 GPIODirModeGet
    0x80008f4c GPIOPinWrite
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX


    Therefore, where the bootstrap code is jumping to is NOT correct. All this is stuff in XDC, deep under the covers, and not anything I can find controls for.

    Now, please explain how these differences occur, and where I can control the something...(XDC, GNU, Project...?) to build the app correctly.

    -CSW

  • Hi CSW,

    Sorry for not being able to help you in the past week. I'll look into this issue and get back to you by the end of this week.

    Thanks for your patience.

    Jianzhong

  • Hi CSW,

    Have you tried loading and running your program through JTAG? If it works with JTAG, it should also work using the bootloader.

    I found a thread that you opened a few years ago: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/662587/compiler-processor-sdk-am335x-creating-binary-file-for-sd-card. This may be what you referred to earlier. Please take a look and see if it applies to your current problem.

    Thanks again for your patience.

    Best regards,

    Jianzhong

  • First, do you know how difficult it is to find stuff from years ago, since E2E erases all my notifications every few days??

    It does load with the JTAG.   And obviously the bootloader doesn't run because the entry point is INT THE WRONG PLACE.  The JTAG forcibly puts the code in DDR and sets the entry point to where the linker requires it.

    The EXAMPLE builds with the entry at 0x800 0000.  But a program with the CCS new project wizard does NOT.   Have you simply tried to use the new project wizard, build an empty program, and look at the map file?

    If there is a statement in the CFG file that is present in the example, but not generated in the new CCS project wizard, I can't find it.

    The old post you mention was placing a new CMD file in the project.... 

    But WHY does the SYSBIOS example not need a CMD file, but the CCS New project does?

    Why is there an obsession to hide how this works, so it's impossible to troubleshoot?

  • Hi Christopher,

    While I let Jianzhong to address your main (remaining) issue, my few inputs on your comments in previous response.

    1. >> The JTAG forcibly puts the code in DDR and sets the entry point to where the linker requires it.

    No - JTAG does not forcibly put the code in DDR.. It is all controlled by the lnk cmd file used for the application. Note that CCS reads the entry symbol and initializes the PC with that address to start the execution.

    2. >>The EXAMPLE builds with the entry at 0x800 0000.  But a program with the CCS new project wizard does NOT

    Note that CCS is not meant only for Processor SDK release. There are various teams across TI, use CCS. So, the PDK example setting up entry point to some value, not necessarily match to CCS project wizard.  Please view them as two different approaches.

    3.  >> If there is a statement in the CFG file that is present in the example, but not generated in the new CCS project wizard, I can't find it.

    Same input as #2. Wizard and PDK Examples are different.

    4.  >> WHY does the SYSBIOS example not need a CMD file, but the CCS New project does?

    As you know, any Program needs the link cmd file to link and generate the final executable. In the SYS BIOS case, the lnk cmd file is generated from the default based on the board (platform) used for building the application. You can see the lnk cmd file used for building the application under the generated Debug folder (in CCS) - There are few depth to it - you can probably grep for the linker command file.

    Sys BIOS provides some flexibility to users, to not use the linker template (default one) and instead user can provide his own template lnk cmd file.  You would need to mention this change in RTSC cfg  file, to have custom link cmd file template. 

    Ref: http://software-dl.ti.com/targetcontent/legacy_files/targetcontent/rtsc/xdctools_3_10/xdctools_3_10_03/exports/docs/cdoc/xdc/cfg/Program.html#xdoc-desc

    Please look for Program.linkTemplate  in above html page. Note that this is java script centric. so you may need to write the template in java script.

    Hope this helps to clarify your questions.

  • Thanks Aravind for the excellent explanations. 

    Christopher,

    I just wanted to add that you can find your older posts by searching. For example, if you put "site:e2e.ti.com Entry Point Address in SYSBIOS am335x" in Google search bar, you should be able to find the thread that I provided earlier.

    Best regards,

    Jianzhong

  • Just an FYI...   45 minutes of a detailed reply to try to get a better understanding....  Was eaten by you web forum popping up "Error, please try again or contact the administrator"

    This process is horrid, and I will not recreate it tonight, while this mad at your service.

  • Sorry about that experience. It must have been very frustrating. The web server can sometimes have hiccups.

  • 'sometimes' ?  This happens routinely (25% of the time).  No one seems to care to fix it.  Or add some kind of auto-save.

  • Here we go again...  Lets hope this one POSTS...

    The subject "How to Set the Entry Point" still mostly applies.  How is it set in the Example, and why is it NOT set in a wizard based project?

    Import an example:

    Build and examine the map file:

    It is correct.

    Change the target from ti.platforms.evmAM3359  to ti.platforms.beaglebone  and rebuild...  NO CHANGE

    Create a SYSBIOS project using the wizard.

    The files are there, auto-generated:

    Build and examine the map file:

    IT IS WRONG.  9The c_int00 code block appears the same size...  but in the wrong place )

    In BOTH cases, the settings are Platform:gnu.targets.arm.A8F   and Target:  ti.platforms.beaglebone

    In BOTH cases, the environment is creating the linker script.  

    in BOTH cases, the XDC is 3.55 and SYSBIOS is 6.76

    In the case that DOES NOT correctly, simply throwing in more "products" in the project settings makes no difference.

    Trying to find what is in the CFG file that is doing it has turned up nothing.

    I can fix the second one ONLY by adding my own CMD file.  But it IS NOT there in the example.

    Last time, my other post helped me fix the entry point by what now appears to be a work-around HACK.

    WHAT IS THE DIFFERENCE between these two projects?

    WHY does one generate a linker script that correctly sets the entry point, and the OTHER project doesn't??

    WHY does it need a HACK?

  • Hi,

    Glad that your post went through this time and thanks for the detailed explanation. 

    WHAT IS THE DIFFERENCE between these two projects?

    If you compare the generated linker command files, linker.cmd, in folder <project root>\Debug\configPkg, you'll notice the difference. The PDK example's linker.cmd has the following as the first section in SECTIONS:

    Fullscreen
    1
    2
    3
    .c_int00 : {
    KEEP (*(.c_int00))
    } > REGION_TEXT
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    However, the linker.cmd generated by the CCS wizard doesn't. 

    WHY does one generate a linker script that correctly sets the entry point, and the OTHER project doesn't??

    I don't know the exact reason, but there is a way to ensure .c_int00 to be placed at the beginning of a section (e.g. DDR2). If you add the following in the app.cfg generated by the CCS wizard, you should have .c_int00 at 0x80000000:

    Fullscreen
    1
    Program.sectMap[".c_int00"] = "DDR2";
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    Hope this helps. Thanks again for your patience.

    Best regards,

    Jianzhong

  • Jianzhong,

    I confirmed that works.

    (I used to be able to insert quotes, now THAT feature is apparently gone from E2E as well...)

    Both linker scripts say This file was generated by linkcmd_bm_v7a.xdt from the gnu.target.arm package

    You say   "I don't know the exact reason, but there is a way to ensure ..."

    So, in summary, no one at TI knows why this is necessary in a wizard generated project, but not in a imported demo, despite them using the same XDC and SYSBIOS versions.  And the script being generated from the same toolset.

    Any wonder why I have such disdain for this environment?  Because it's doing things I can't control, it doesn't do things consistently, and the only solutions I get are to use hacks to get around it.

    I was told once "don't start with an empty project, use an example"...   Well that's only useful if the ultimate project is going to use JUST a flashing led, or JUST do a SPI communication, or JUST access fat32...  Not if I need more than one. 

    Then the examples have other things buried in there I have to figure out how to rip out as they are bloat.

    I am trying to convert a project that is hundreds of source code files, and hundreds of thousands of lines from the old TI complier to the GNU because TI won't support their own compiler in Sitara anymore.  I can't do that by simple "starting with an example project".