Part Number: TDA4VM
Hi Sir :
I want to disable automatic mount EMMC partition 0 to /run/media/mmcblk0p1.
How should I set it?
PSDK version 7.3.0

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
Hi Sir :
I want to disable automatic mount EMMC partition 0 to /run/media/mmcblk0p1.
How should I set it?
PSDK version 7.3.0

Hi,
Can you try disabling the main_sdhci0 node from the kernel dts?
Something like below:
diff --git a/arch/arm64/boot/dts/ti/k3-j721e-common-proc-board.dts b/arch/arm64/boot/dts/ti/k3-j721e-common-proc-board.dts
index d1a2eb415..ae8b0e6b1 100644
--- a/arch/arm64/boot/dts/ti/k3-j721e-common-proc-board.dts
+++ b/arch/arm64/boot/dts/ti/k3-j721e-common-proc-board.dts
@@ -771,6 +771,7 @@
non-removable;
ti,driver-strength-ohm = <50>;
disable-wp;
+ status = "disabled";
};
&main_sdhci1 {
Best Regards,
Keerthy
Hi,
Then you are using filesystem in eMMC? Typically SD is used as file system.
Can you try:
env default -a
saveenv
in the u-boot prompt so that MMC-SD is used as the default file system?
Best Regards,
Keerthy
Hi Keerthy:
Currently TDA4VM needs to use fast boot , so SD Card will not be used.
Optimized flow involve SBL -> A72 ATF/OPTEE -> A72 Linux Kernel
Use Device : OSPI Flash and eMMC
Hi Pierre,
Then you need eMMC for file system then what is that you want to achieve?
I want to disable automatic mount EMMC partition 0 to /run/media/mmcblk0p1.
This is the partition where we have the file system then why do you want to disable?
- Keerthy
Hi Keerthy:
Currently I need TDA4VM to fast boot, but I don't need to auto-mount "/dev/mmcblk0p1".
I will mount it after the App access.
Hi Pierre,
Without getting to Linux command prompt how are you loading the App?
Some sort of command line is needed isn't it?
- Keerthy