This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Champs,
SW: 08_00_06_11
Customer is using emmc boot, he found that the non file partitions are always mounted under /run/media/mmcblk*p*. He tried to modify the /etc/udev/rules.d/local.rule和/etc/fstab, but it doesn't work.
The emmc non system partitions are automatically mounted in /run/media/ directory.
Customer wanted to mount /dev/mmcblk0p* in self defined directory, he tried add entrance in fstab, but it failed.
Thanks
Regards
Shine
HI shine
Please remove noauto and replace it with the auto it should work.
Thanks
Diwakar