This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello ,
I am working on beaglebone and boot linux via eMMC
i can see 4 partitions under /dev
root@beaglebone:/# mount /dev/mmcblk0
mmcblk0 mmcblk0boot0 mmcblk0boot1 mmcblk0p1 mmcblk0p2
i can mount mmcblk0p1 mmcblk0p2 without any problem
But i can not able to mount mmcblk0boot1 or mmcblk0boot0 . . why ?
i get the below error
root@beaglebone:/# mount /dev/mmcblk0boot0 /mnt/boot0/
mount: /dev/mmcblk0boot0 is write-protected, mounting read-only
[ 135.922967] F2FS-fs (mmcblk0boot0): Can't find a valid F2FS filesystem
mount: wrong fs type, bad option, bad superblock on /dev/mmcblk0boot0,
missing codepage or helper program, or other error
In some cases useful info is found in syslog - try
dmesg | tail or so.
Thanks
Kiran
Hello Kiran,
There is not a valid F2FS filesystem on that partition.
Best regards,
Kemal