Hi Ti,
We are using SDK 07.01.00.18, and we connected AM6548 and another master with EEPROM on I2C0.
And there is a reset pin for us to control another master.
In this case, when reset pin is high, EEPROM only can communication with another master, it cannot communication with AM6548. This is ok.
But if the reset pin is low, EEPROM cannot communicate with AM6548.
After we disconnect the i2c between another master and EEPROM, AM6548 can communicate with EEPROM.
We want to know if AM6548 support multi master feature on the same i2c bus?
How can we do this?
Thanks.
Eric