Hi:
I would have tagged onto these other two threads, but I have slightly different error messages.
EVM rev PROC101A (001)
I followed every step in this document to the letter, on Ubuntu 18.04
Two things I noticed that seemed slightly out of the ordinary is that:
- for the uart to work on Ubuntu, you have to chmod 666 /dev/ttyUSB0
- The version of CCS specified in the Getting Started manual (10.3.1) is not available, it is now 10.4
Anyhow the bootloader progamming all worked and in CCS I got this on the terminal:
Starting NULL Bootloader ...
DMSC Firmware Version 21.5.0--v2021.05 (Terrific Llam
DMSC Firmware revision 0x15
DMSC ABI revision 3.1
INFO: Bootloader_runCpu:147: CPU r5f1-0 is initialized to 800000000 Hz !!!
INFO: Bootloader_runCpu:147: CPU r5f1-1 is initialized to 800000000 Hz !!!
INFO: Bootloader_runCpu:147: CPU m4f0-0 is initialized to 400000000 Hz !!!
INFO: Bootloader_runCpu:147: CPU a530-0 is initialized to 800000000 Hz !!!
INFO: Bootloader_runCpu:147: CPU a530-1 is initialized to 800000000 Hz !!!
INFO: Bootloader_loadSelfCpu:199: CPU r5f0-0 is initialized to 800000000 Hz !!!
INFO: Bootloader_loadSelfCpu:199: CPU r5f0-1 is initialized to 800000000 Hz !!!
INFO: Bootloader_runSelfCpu:216: All done, reseting self ...
When I launch the configuration, I get this error after a long wait:
CS_DAP_0: Error initializing emulator: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the XDS110SupportReadMe.pdf file there for instructions. (Emulation package 9.4.0.00129)
Retrying yields same result, but immediately.
I read and tried the workaround here:
However, it never works.
Pretty much stuck at this point.
Thank you
Howard