Other Parts Discussed in Thread: OMAPL138
I'm having issues setting up an empty project.
What might be causing the issue of:
**** Build of configuration Debug for project demo **** "C:\\ti\\ccs1040\\ccs\\utils\\bin\\gmake" -k -j 16 all -O Building file: "../main.c" Invoking: C6000 Compiler "C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-c6000_8.3.11/bin/cl6x" -mv6740 --include_path="/packages/ti/drv/gpio" --include_path="/packages" --include_path="D:/Users/Daniel Vong/Documents/workspace_v10/demo" --include_path="C:/ti/ccs1040/ccs/tools/compiler/ti-cgt-c6000_8.3.11/include" --define=c6748 -g --diag_warning=225 --diag_wrap=off --display_error_number --preproc_with_compile --preproc_dependency="main.d_raw" "../main.c" >> Compilation failure subdir_rules.mk:9: recipe for target 'main.obj' failed "../main.c", line 2: fatal error #1965: cannot open source file "ti/drv/gpio/GPIO.h" 1 catastrophic error detected in the compilation of "../main.c". Compilation terminated. gmake: *** [main.obj] Error 1 gmake: Target 'all' not remade because of errors. **** Build Finished ****
End goal is to integrate with third party source code.
Is there a private link where I can send the source code to?
Regards,
Daniel