This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Is the internal Pullup/Pulldown enabled in SBL (Secondary Boot Loader)?
Is there an intermediate potential and through current between device power-up and internal pullup/pulldown enabled (until SBL processing is complete)?
Does this damage the device?
Thanks and Best regards,
Tsurumoto.
The default state of the internal PU or PD is defined in the data manual, and is enabled by the ROM (prior to SBL). It is possible the SBL adjust the default configuration (software teams can confirm). There is not an intermediate state with both PU and PD is enabled (at power up), and it would not damage the device.
The resistance value is 15K to 30K-ohms for both PU and PD
Hi
I got additional question about it.
1)
After SBL, if Hi-Z input pins or Hi-Z bidirectional pins are an intermediate potential and through current
then it damages the device?
1) It is recommended to avoid 'floating' inputs as it is possible pins can be damaged. Pins should not be held at intermediate state.
2) No - should be OK enabling PU/PD at SBL.
3) Yes, pull value can be less than 4.7kOhms. If setting as output (to over-drive PU/PD), just make sure IO max current is not exceeded.