This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
A customer intends to do PCIe communication between the TDA4VM chip and another chip under a QNX system based on a linux system, and the customer would like to know if there is a sample code on the QNX side.
Could you help check this case? Thanks!
Best Regards,
Cherry
Hi KB,
Thanks for your reply.
The customer also would like to know is it possible to provide the drivers under linux, they needs to know more about the register configuration of the PCIe this section.
Thanks and Best Regards,
Cherry
Hi,
May I know is there any updates about the additional questions?
Thanks and Best Regards,
Cherry
Hi Cherry,
The linux PCIe driver is provided as part of the PSDK Linux release available at PROCESSOR-SDK-J721E Software development kit (SDK) | TI.com.
The SDK 8.0 documentation contains the following sections related to PCIe
3.2.2.10. PCIe End Point — Processor SDK Linux for J721e Documentation
3.2.2.11. PCIe Backplane — Processor SDK Linux for J721e Documentation
3.2.2.12. PCIe Root Complex — Processor SDK Linux for J721e Documentation
Regards,
kb
Igor:
Yes about the Linux driver.
But will let Kip to answer about QNX solution for DRA821.
Jian
Regarding:
Does the same answer goes for DRA821 PCIe with QNX? (contact QNX etc ...)
Yes, the DRA821 PCIe framework for DRA821 is a QNX/Blackberry deliverable.
Regards,
kb