In IBIS, there are many mode choice, especially for DDR, some item is not clear to user, for example between Model_479 and Model_480,RExt and Tolerance have different value, how to determine which to use?
I understand the Tolerance is system DDR power supply voltage drift rate, we can measure on the board, am I right?
But what is input load/RExt? how to determine and how to configure it in software(EMIF configuration tool excel) or hardware?
Model_479
Direction = Input
Voltage = 1.5V
Input load = FULLTERM, 0.88 * RExt = 1.125 * Iout (I[2:0] = "100"), 9mA nominal with Rext = 50R
Temperature range = Industrial temperature range (-40C to 125C, 25C nominal)
Tolerance = 10% power supply tolerance
Model_480
Direction = Input
Voltage = 1.5V
Input load = FULLTERM, 1.14 * RExt = 0.875 * Iout (I[2:0] = "010"), 7mA nominal with Rext = 50R
Temperature range = Industrial temperature range (-40C to 125C, 25C nominal)
Tolerance = 5% power supply tolerance