Hi Team,
I see a very weird issue of networking on AM335x-GP-EVM and AM335x-SK, with ti-rt-linux-5.4.y version.
The RX count is always zero on eth0.The TX count increases. The Network never comes up, as there is no handshake of network packets is happening.
The same target Hardware with ti-rt-linux-4.19.y, works without issue.
When I looked at the dts files, I could see the following
5.4 on the right and 4.19rt on the left
When I modified it to the following:
It works. Can you please let me know what is the correct value for the phy-mode. How it is decided?
On AM437x-evm the phy-mode = "rgmii", across multiple kernel versions.
The networking works fine on AM437x-GP-EVM.