Other Parts Discussed in Thread: TEST, DRA821, TDA4
Dear support,
For DDR ECC per-load, we use the BIST engine for SDRAM initilization, but it fails, the following is the registers configured,
Could you help me check whether the configuration is Ok?
I want to initialize the 0x9000 0000 ~ 0x9000 03FF(1KB)
/* BIST start address 0.*/
Tst_DDR_CTL->DENALI_CTL_196 = 0x90000000;
/* BIST start address 1.*/
Tst_DDR_CTL->DENALI_CTL_197 = 0x00000000;
/* BIST test mode.*/
/* 4 - memory initialization. */
Tst_DDR_CTL->DENALI_CTL_200 = 0x4;
/* BIST data pattern 0.*/
Tst_DDR_CTL->DENALI_CTL_201 = 0x55AA55AA;
/* BIST data pattern 1.*/
Tst_DDR_CTL->DENALI_CTL_202 = 0x55AA55AA;
/* BIST data pattern 2.*/
Tst_DDR_CTL->DENALI_CTL_203 = 0x55AA55AA;
/* BIST data pattern 3.*/
Tst_DDR_CTL->DENALI_CTL_204 = 0x55AA55AA;
/* bit0 -BIST GO */
/* bit18 -21, the number of address bits during BIST operation. */
/* 9 - represent 1KB .*/
Tst_DDR_CTL->DENALI_CTL_194 |= 0x90001;