This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello it is 3 weeks, can you please share with us update of the issue?
Hi,
Sorry for the delay.
Unfortunately, I am not able to reproduce the issue. Can you elaborate on the your setup and steps to reproduce the issue.
Regards,
Tanmay
We are working on easier way of reproducing this and will get to you.
Hi Tanmay,
There are exact steps how to reproduce
Simple example "example.c" is attached. Example contains steps mentioned above for eth1 interface.
Compile and run the example on TMDX654IDKEVM to reproduce the bug.
Regards,
Lukas
#include <errno.h> #include <error.h> #include <linux/ethtool.h> #include <linux/if_packet.h> #include <linux/netlink.h> #include <linux/rtnetlink.h> #include <linux/sockios.h> #include <net/if.h> #include <stdbool.h> #include <stdio.h> #include <stdint.h> #include <stdlib.h> #include <string.h> #include <sys/ioctl.h> #include <sys/socket.h> #include <sys/types.h> #include <unistd.h> int nwords; uint8_t commData[sizeof(struct ethtool_link_settings) + 3 * 4 * 4]; // struct + 3 * 32/8 * nwords -> allocate for nwords <= 4 struct ethtool_link_settings *data = (struct ethtool_link_settings *)commData; /* Get interface state with link mode, store them to data */ static void getLinkSettings(int fd, const char* devname) { int ret; struct ifreq ifr; memset(&ifr, 0, sizeof(ifr)); strncpy(ifr.ifr_name, devname, IFNAMSIZ); ifr.ifr_data = (char *)data; data->link_mode_masks_nwords = nwords; data->cmd = ETHTOOL_GLINKSETTINGS; ret = ioctl(fd, SIOCETHTOOL, &ifr); if (ret < 0) { error(-53, errno, "Cannot get link settings"); } } /* Do ethtool api handshake and obtain current nwords */ void getNwords(int fd, const char* devname, int* nwords) { int ret; struct ifreq ifr; struct ethtool_link_settings handshake; memset(&ifr, 0, sizeof(ifr)); strncpy(ifr.ifr_name, devname, IFNAMSIZ); ifr.ifr_data = (char *)(&handshake); handshake.cmd = ETHTOOL_GLINKSETTINGS; ret = ioctl(fd, SIOCETHTOOL, &ifr); if (ret < 0) { error(-53, errno, "Failed ethtool handshake"); } // Validate nwords, expected is negative value if (handshake.link_mode_masks_nwords >= 0 || handshake.cmd != ETHTOOL_GLINKSETTINGS) { error(-53, errno, "Ethtool handshake wrong value"); } *nwords = abs(handshake.link_mode_masks_nwords); } /* Init netlink socket for ethtool */ int initNetlinkSocket(const char* devname) { int fd; int ret; struct sockaddr_nl sa_nl; // open socket for netlink fd = socket(AF_NETLINK, SOCK_RAW, NETLINK_ROUTE); if (fd < 0) { error(-53, errno, "Cannot get netlink socket"); } memset(&sa_nl, 0, sizeof(sa_nl)); sa_nl.nl_family = AF_NETLINK; sa_nl.nl_groups = RTMGRP_LINK; // bind netlink socket ret = bind(fd, (struct sockaddr *)&sa_nl, sizeof(sa_nl)); if (ret == -1) { error(-53, errno, "Netlink socket bind failed"); } getNwords(fd, devname, &nwords); return fd; } /* Set administrative link state */ void setAdminLinkState(int fd, const char* devname, bool up) { int ret; struct ifreq ifr; memset(&ifr, 0, sizeof(ifr)); strncpy(ifr.ifr_name, devname, IFNAMSIZ); // get current state of flasg ret = ioctl(fd, SIOCGIFFLAGS, &ifr); if (ret < 0) { error(-53, errno, "Cannot get administrative link state"); } // set requested link state if (up) { ifr.ifr_flags |= IFF_UP; } else { ifr.ifr_flags &= ~IFF_UP; } // write to device ret = ioctl(fd, SIOCSIFFLAGS, &ifr); if (ret < 0) { error(-53, errno, "Cannot set administrative link state"); } } int main() { char* iface = "eth1"; int nlFd = initNetlinkSocket(iface); setAdminLinkState(nlFd, iface, false); getLinkSettings(nlFd, iface); }
Hi Lukas,
I discussed this with my colleagues and found out that this is not a bug. When a link down issued, we disconnect the phy itself. Hence the query to get the link setting fails after a link down. I am not sure why it worked for you in SDK 8.0 in first place.
This is not planned to be changed in near future. So, I would like to know the need and involvement of this feature in your project so that we can look for a workaround/solution for this.
Regards,
Tanmay
Hi Tanmay,
When you set link down you are not able to neither get nor set supported MAU types, this behavior is not good.
Also when you set MAU types and do link down and link up, then the interface is in "default" and does not has previous configuration.
Our usage of this is set link settings when is link down and then set link up. Only this procedure ensure link establishing with requested configuration. It correctly worked on SDK 8.0 and older versions. Now the interface behaves differently than all other systems.
Regards,
Lukas
Hello Tanmay,
for starters, I have to point out that the PHY disconnection you mentioned is merely a cause of the bug, and by no means a reason why this behavior would not be a bug.
To wit:
Those are two reasons why this issue is definitely a bug.
Because we now cannot start the link with defined state. We simply have no way to set MAU type and link up atomically, and this bug took the possibility to set MAU type before link up away from us.
Since our project is extremely sensitive to detailed behavior of our link partner, starting the link and only then changing the MAU type is option that may not even be acceptable for us.
Currently, this bug prevents us from updating our software base from SDK 8.0 upwards, thus preventing us from using any fixes of TI bugs that already appeared in newer releases. Some of these fixes are necessary for features in our current project timeline, so this bug may happen to actually stall the whole project.
Attempt to workaround this bug would cost us several manweeks and discussions with multiple external parties at best.
At worst, it would prove impossible.
I, personally, see at least two of them:
First: Just keep the PHY connected after link down. This looks like the most simple, while completely correct solution from my perspective (I know no details of your implementation).
Second: Before disconnecting the PHY, load its relevant state into the driver and turn the PHY down to a state, where it cannot interact with a link partner. Then, as long as PHY is disconnected, manage the PHY state in the driver. Finally, when the PHY is connected, save the state kept in driver into it and then forward the set calls as usual.
None of those solutions seems difficult or complex to invent or implement, but they need to be done on the driver side inside kernel, which rules out any solution in application, which simply does not have any fine controls over PHY.
I hope this post made some things clear and helped us to align our viewpoints.
Hopefully, it will also help you to plan the fix for this bug into near future.
Best Regards,
Jan
I have reported one more issue which might be related:
TMDX654IDKEVM: Linux-RT SDK 8.2: 'ethtool -s eth1 speed 1000 duplex full autoneg on' does not work for eth1-eth5
Hi Jan, Lukas,
Thanks for the explanation. It was very clear and helpful. The issue is indeed something which has to be fixed. Hence, I have filed an internal ticket for it (https://jira.itg.ti.com/browse/LCPD-27922).
I will update you on the progress as soon as we have a fix.
Regards,
Tanmay
The fix for this is available in our official ti-linux-5.10.y branch, so it would be part of any upcoming AM65x Processor SDK release (v8.3 or later):
Regards, Andreas