We found a problem with selecting the desired pins for the EHRPWM1 outputs. Based on the DM it should be possible to output e.g. EHRPWM1A at 3 different pins (D12, D14, L1), but looks like the MCAL configuration (mcal_config_01_09_00_30) only supports to select pin D12 (gpmc_ben0).
The DRA78x device is used in different version of an audio amplifier and the identical SBL will be used on all version, therefore pinmux settings are excluded from SBL and instead an AUTOSAR application needs to configure the pinmux settings depending on the version. Therefore it's needed to allow the selection of all possible pins for the PWMSS output signals. What's needed to get this done? Will that require changes in the mcal_config_01_09_00_30 software package?
Best regards,
Manfred