Other Parts Discussed in Thread: AM4378,
If the MPU AM4378 is configured as CPSW, and one RJ45 (J6 in the TMDXSK437X EVM) is connected with TCP/IP ethernet, the other RJ45 (J8 in the TMDXSK437X EVM) is connected with Ethercat. Dose the MPU can communicate with TCP/IP ethernet and Ethercat simultaneously ? If the answer is NO, how can I configure the MPU to communicate with TCP/IP ethernet and Ethercat simultaneously?