Part Number: TMDS64GPEVM
Hi All,
I am having ongoing issues with dropped pings while running the LwIP / free RTOS example.
Compiler: CCS Version: 11.1.0.0001
SDK: mcu_plus_sdk_am64x_08_01_00_36
Hardware: AM64x Evaluation Module TMDS64GPEVM
Below is the terminal view of boot message and startup of the example
And here is the result of an attempt to ping the EVM:
Any help with this would be appreciated.
Thanks, Joel