Part Number: AM625
The fields of the OLDI IO_CTRL registers are not fully defined in the TRM, SPRUIV7 - May 2022. For example, bits 16-19 of OLDI0_CLK_IO_CTRL are described only as "Controls LVDS Transmitter TXDRV". Also, the reset value for that is listed as "64h" but it is only a 4-bit field. (The leading '6' appears to be incorrect.)
Please provide complete definitions for all fields of all OLDI IO_CTRL register. Also, please indicate whether the reset values listed in the SPRUIV7 result in OLDI (LVDS) signals being enabled by default on the corresponding AM62x pins, assuming that their pin muxes have been configured correctly.