Is any of the following permissible with the EMIF:
- Within a byte, DQ signals can be swapped
- Bytes can be swapped (all signals DQ, DQS, DM have to be swapped)
- DQ signal should not be swapped between bytes (e.g. DQ0 going into DQS1 group)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is any of the following permissible with the EMIF:
Also, is it permissible to swap address lines?
Hi Andrew,
Yes, when TDA3x is interfaced to DDR3:
I do not think the address pins (A15:0) or bank address pins (BA2:0) can be swapped. I believe these are used to program the DDR3 mode registers (inside the DRAM), and there is no way to re-map the address pin to function inside the TDA3x controller.
Regards,
Kevin