Other Parts Discussed in Thread: AM4377
Presently working on AM437x-HS custom board, Keep sending data to UART1 without input flush or read operations,Observed that,the OS freezes at some point, power cycle or reset is the only way to bring back board Normal operation.
Help me out further debug and proper solution.
Used SDK : TI-SDK-07_03_00_005
Here attached Debug Log for further reference.
U-Boot SPL 2019.01 (May 04 2022 - 11:26:25 +0000)
SPL BOOT DEVICE: a
SPL: Unsupported Boot Device!
SPL BOOT DEVICE: 7
Trying to boot from MMC1
MMC DEVICE INDEX: 7
Card did not respond to voltage select!
spl: mmc init failed with error: -95
SPL BOOT DEVICE: 8
Trying to boot from MMC2
MMC DEVICE INDEX: 8
Authentication passed
Authentication passed
U-Boot 2019.01 (May 04 2022 - 11:26:25 +0000)
CPU : AM437X-HS rev 1.2
Model: TI AM437x GP EVM
DRAM: 1 GiB
PMIC: TPS65218
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Loading Environment from FAT... Card did not respond to voltage select!
Net:
Warning: ethernet@4a100000 using MAC address from ROM
eth0: ethernet@4a100000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
1556 bytes read in 2 ms (759.8 KiB/s)
Running bootscript from mmc1 ...
## Executing script at 90000000
Card did not respond to voltage select!
SD/MMC Found On Device 0
Card did not respond to voltage select!
Card did not respond to voltage select!
starting USB...
USB0: Register 2000440 NbrPorts 2
Starting the controller
USB XHCI 1.00
scanning bus 0 for devices... 1 USB Device(s) found
scanning usb for storage devices... 0 Storage Device(s) found
Device 0: unknown device
Running from eMMC
switch to partitions #0, OK
mmc1(part 0) is current device
4710912 bytes read in 240 ms (18.7 MiB/s)
70644 bytes read in 4 ms (16.8 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffeb000, end 8ffff3f3 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 5.4.106-ts-armv7l (khbuild@4b30077d30ce) (gcc version 6.5.0 (Timesys 20220222)) #4 PREEMPT Wed Jul 20 12:27:51 2
[ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: TI AM437x GP EVM
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 48 MiB at 0xba800000
[ 0.000000] On node 0 totalpages: 262144
[ 0.000000] Normal zone: 1728 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 196608 pages, LIFO batch:63
[ 0.000000] HighMem zone: 65536 pages, LIFO batch:15
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM437x ES1.2 (sgx neon)
[ 0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
[ 0.000000] pcpu-alloc: [0] 0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 260416
[ 0.000000] Kernel command line: console=ttyS0,115200 root=/dev/mmcblk1p5 rootfstype=ext4 rw early_printk loglevel=8 rootwait
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 941436K/1048576K available (9216K kernel code, 303K rwdata, 3300K rodata, 1024K init, 257K bss, 57988K reserved, 4915)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] L2C: platform modifies aux control register: 0x0e030000 -> 0x3e430000
[ 0.000000] L2C: DT/platform modifies aux control register: 0x0e030000 -> 0x3e430000
[ 0.000000] L2C-310 enabling early BRESP for Cortex-A9
[ 0.000000] OMAP L2C310: ROM does not support power control setting
[ 0.000000] L2C-310 dynamic clock gating disabled, standby mode disabled
[ 0.000000] L2C-310 cache controller enabled, 16 ways, 256 kB
[ 0.000000] L2C-310: CACHE_ID 0x410000c9, AUX_CTRL 0x4e430000
[ 0.000000] random: get_random_bytes called from start_kernel+0x2b0/0x45c with crng_init=0
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000012] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000029] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000038] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000473] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000482] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000975] Console: colour dummy device 80x30
[ 0.001038] Calibrating delay loop... 1987.37 BogoMIPS (lpj=9936896)
[ 0.060189] pid_max: default: 32768 minimum: 301
[ 0.060388] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)
[ 0.060414] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)
[ 0.061307] CPU: Testing write buffer coherency: ok
[ 0.061366] CPU0: Spectre v2: using BPIALL workaround
[ 0.062253] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.062398] rcu: Hierarchical SRCU implementation.
[ 0.062484] EFI services will not be available.
[ 0.062980] devtmpfs: initialized
[ 0.074284] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[ 0.074689] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.074710] futex hash table entries: 256 (order: -1, 3072 bytes, linear)
[ 0.078162] pinctrl core: initialized pinctrl subsystem
[ 0.078920] DMI not present or invalid.
[ 0.079376] NET: Registered protocol family 16
[ 0.081153] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.105809] cpuidle: using governor ladder
[ 0.105844] cpuidle: using governor menu
[ 0.126408] No ATAGs?
[ 0.126428] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[ 0.126444] hw-breakpoint: maximum watchpoint size is 4 bytes.
[ 0.142802] debugfs: Directory '49000000.edma' with parent 'dmaengine' already present!
[ 0.142830] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.143581] reg-fixed-voltage fixedregulator-v3_3d: GPIO lookup for consumer (null)
[ 0.143593] reg-fixed-voltage fixedregulator-v3_3d: using device tree for GPIO lookup
[ 0.143616] of_get_named_gpiod_flags: can't parse 'gpios' property of node '/fixedregulator-v3_3d[0]'
[ 0.143630] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator-v3_3d[0]'
[ 0.143642] reg-fixed-voltage fixedregulator-v3_3d: using lookup tables for GPIO lookup
[ 0.143651] reg-fixed-voltage fixedregulator-v3_3d: No GPIO consumer (null) found
[ 0.143924] reg-fixed-voltage fixedregulator-mmcwl: GPIO lookup for consumer (null)
[ 0.143936] reg-fixed-voltage fixedregulator-mmcwl: using device tree for GPIO lookup
[ 0.143952] of_get_named_gpiod_flags: can't parse 'gpios' property of node '/fixedregulator-mmcwl[0]'
[ 0.143978] reg-fixed-voltage fixedregulator-mmcwl: No GPIO consumer (null) found
[ 0.144889] iommu: Default domain type: Translated
[ 0.147112] SCSI subsystem initialized
[ 0.147612] mc: Linux media interface: v0.10
[ 0.147649] videodev: Linux video capture interface: v2.00
[ 0.147761] pps_core: LinuxPPS API ver. 1 registered
[ 0.147768] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.147788] PTP clock support registered
[ 0.147821] EDAC MC: Ver: 3.0.0
[ 0.148965] Advanced Linux Sound Architecture Driver Initialized.
[ 0.150137] clocksource: Switched to clocksource timer1
[ 0.157544] thermal_sys: Registered thermal governor 'fair_share'
[ 0.157552] thermal_sys: Registered thermal governor 'bang_bang'
[ 0.157566] thermal_sys: Registered thermal governor 'step_wise'
[ 0.157572] thermal_sys: Registered thermal governor 'user_space'
[ 0.157578] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.158202] NET: Registered protocol family 2
[ 0.158904] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes, linear)
[ 0.158935] TCP established hash table entries: 8192 (order: 3, 32768 bytes, linear)
[ 0.158996] TCP bind hash table entries: 8192 (order: 3, 32768 bytes, linear)
[ 0.159068] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.159243] UDP hash table entries: 512 (order: 1, 8192 bytes, linear)
[ 0.159270] UDP-Lite hash table entries: 512 (order: 1, 8192 bytes, linear)
[ 0.159430] NET: Registered protocol family 1
[ 0.160019] RPC: Registered named UNIX socket transport module.
[ 0.160030] RPC: Registered udp transport module.
[ 0.160036] RPC: Registered tcp transport module.
[ 0.160041] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.160054] PCI: CLS 0 bytes, default 64
[ 0.162102] Initialise system trusted keyrings
[ 0.162413] workingset: timestamp_bits=14 max_order=18 bucket_order=4
[ 0.166976] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.167743] NFS: Registering the id_resolver key type
[ 0.167778] Key type id_resolver registered
[ 0.167784] Key type id_legacy registered
[ 0.167831] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.168518] Key type asymmetric registered
[ 0.168531] Asymmetric key parser 'x509' registered
[ 0.168580] bounce: pool size: 64 pages
[ 0.168629] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[ 0.168639] io scheduler mq-deadline registered
[ 0.168645] io scheduler kyber registered
[ 0.173438] gpio gpiochip0: (gpio-0-31): added GPIO chardev (254:0)
[ 0.173554] gpiochip_setup_dev: registered GPIOs 0 to 31 on device: gpiochip0 (gpio-0-31)
[ 0.173603] OMAP GPIO hardware version 0.1
[ 0.197209] gpio gpiochip1: (gpio-32-63): added GPIO chardev (254:1)
[ 0.197298] gpiochip_setup_dev: registered GPIOs 32 to 63 on device: gpiochip1 (gpio-32-63)
[ 0.199669] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.216701] gpio gpiochip2: (gpio-64-95): added GPIO chardev (254:2)
[ 0.216803] gpiochip_setup_dev: registered GPIOs 64 to 95 on device: gpiochip2 (gpio-64-95)
[ 0.218204] gpio gpiochip3: (gpio-96-127): added GPIO chardev (254:3)
[ 0.218286] gpiochip_setup_dev: registered GPIOs 96 to 127 on device: gpiochip3 (gpio-96-127)
[ 0.223719] gpio gpiochip4: (gpio-128-159): added GPIO chardev (254:4)
[ 0.223808] gpiochip_setup_dev: registered GPIOs 128 to 159 on device: gpiochip4 (gpio-128-159)
[ 0.225183] gpio gpiochip5: (gpio-160-191): added GPIO chardev (254:5)
[ 0.225262] gpiochip_setup_dev: registered GPIOs 160 to 191 on device: gpiochip5 (gpio-160-191)
[ 0.235622] pinctrl-single 44e10800.pinmux: 199 pins, size 796
[ 0.285590] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.289256] omap8250 44e09000.serial: No clock speed specified: using default: 48000000
[ 0.290049] printk: console [ttyS0] disabled
[ 0.290247] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 66, base_baud = 3000000) is a 8250
[ 1.144733] printk: console [ttyS0] enabled
[ 1.149684] omap8250 48022000.serial: No clock speed specified: using default: 48000000
[ 1.158541] omap8250 48022000.serial: GPIO lookup for consumer rts
[ 1.164825] omap8250 48022000.serial: using device tree for GPIO lookup
[ 1.171545] of_get_named_gpiod_flags: parsed 'rts-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@0/target-module@22)
[ 1.186569] gpio gpiochip4: Persistence not supported for GPIO 16
[ 1.192736] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 73, base_baud = 3000000) is a 8250
[ 1.202136] omap8250 48024000.serial: No clock speed specified: using default: 48000000
[ 1.210951] omap8250 48024000.serial: GPIO lookup for consumer rts
[ 1.217167] omap8250 48024000.serial: using device tree for GPIO lookup
[ 1.223909] of_get_named_gpiod_flags: parsed 'rts-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@0/target-module@24)
[ 1.238889] gpio gpiochip4: Persistence not supported for GPIO 20
[ 1.245077] 48024000.serial: ttyS2 at MMIO 0x48024000 (irq = 74, base_baud = 3000000) is a 8250
[ 1.254491] omap8250 481a6000.serial: No clock speed specified: using default: 48000000
[ 1.263290] omap8250 481a6000.serial: GPIO lookup for consumer rts
[ 1.269505] omap8250 481a6000.serial: using device tree for GPIO lookup
[ 1.276248] of_get_named_gpiod_flags: parsed 'rts-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@100000/target-modu)
[ 1.291704] gpio gpiochip3: Persistence not supported for GPIO 21
[ 1.297852] 481a6000.serial: ttyS3 at MMIO 0x481a6000 (irq = 80, base_baud = 3000000) is a 8250
[ 1.307234] omap8250 481a8000.serial: No clock speed specified: using default: 48000000
[ 1.316049] omap8250 481a8000.serial: GPIO lookup for consumer rts
[ 1.322323] omap8250 481a8000.serial: using device tree for GPIO lookup
[ 1.329005] of_get_named_gpiod_flags: parsed 'rts-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@100000/target-modu)
[ 1.344458] gpio gpiochip1: Persistence not supported for GPIO 5
[ 1.350562] 481a8000.serial: ttyS4 at MMIO 0x481a8000 (irq = 81, base_baud = 3000000) is a 8250
[ 1.359930] omap8250 481aa000.serial: No clock speed specified: using default: 48000000
[ 1.368733] omap8250 481aa000.serial: GPIO lookup for consumer rts
[ 1.375011] omap8250 481aa000.serial: using device tree for GPIO lookup
[ 1.381722] of_get_named_gpiod_flags: parsed 'rts-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@100000/target-modu)
[ 1.397134] gpio gpiochip1: Persistence not supported for GPIO 7
[ 1.403207] 481aa000.serial: ttyS5 at MMIO 0x481aa000 (irq = 82, base_baud = 3000000) is a 8250
[ 1.414619] omap_rng 48310000.rng: Random Number Generator ver. 20
[ 1.421395] random: fast init done
[ 1.425143] random: crng init done
[ 1.449111] brd: module loaded
[ 1.462032] loop: module loaded
[ 1.471100] spi-nor spi0.0: sst25vf016b (2048 Kbytes)
[ 1.476207] 1 fixed-partitions partitions found on MTD device spi0.0
[ 1.482683] Creating 1 MTD partitions on "spi0.0":
[ 1.487504] 0x000000000000-0x000000200000 : "mlo"
[ 1.502344] mdio_bus fixed-0: GPIO lookup for consumer reset
[ 1.508044] mdio_bus fixed-0: using lookup tables for GPIO lookup
[ 1.514263] mdio_bus fixed-0: No GPIO consumer reset found
[ 1.519789] libphy: Fixed MDIO Bus: probed
[ 1.527710] mdio_bus 4a101000.mdio: GPIO lookup for consumer reset
[ 1.533988] mdio_bus 4a101000.mdio: using device tree for GPIO lookup
[ 1.540490] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp@44000000/interconnect@4a000000/segment@0/target-mo'
[ 1.556053] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp@44000000/interconnect@4a000000/segment@0/target-mod'
[ 1.571523] mdio_bus 4a101000.mdio: using lookup tables for GPIO lookup
[ 1.578168] mdio_bus 4a101000.mdio: No GPIO consumer reset found
[ 1.640174] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 1.647870] libphy: 4a101000.mdio: probed
[ 1.652729] mdio_bus 4a101000.mdio:00: GPIO lookup for consumer reset
[ 1.659207] mdio_bus 4a101000.mdio:00: using device tree for GPIO lookup
[ 1.666034] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp@44000000/interconnect@4a000000/segment@0/target-mo'
[ 1.682954] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp@44000000/interconnect@4a000000/segment@0/target-mod'
[ 1.699759] mdio_bus 4a101000.mdio:00: using lookup tables for GPIO lookup
[ 1.706711] mdio_bus 4a101000.mdio:00: No GPIO consumer reset found
[ 1.713537] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8710/LAN8720
[ 1.722913] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 1.729299] cpsw 4a100000.ethernet: ALE Table size 1024
[ 1.734661] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
[ 1.741908] cpsw 4a100000.ethernet: Detected MACID = 24:76:25:cd:19:91
[ 1.750382] i2c /dev entries driver
[ 1.756754] cpuidle: enable-method property 'ti,am4372' found operations
[ 1.764264] sdhci: Secure Digital Host Controller Interface driver
[ 1.770517] sdhci: Copyright(c) Pierre Ossman
[ 1.776142] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 1.782224] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 1.788818] of_get_named_gpiod_flags: parsed 'cd-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@0/target-module@600)
[ 1.803429] gpio gpiochip3: Persistence not supported for GPIO 14
[ 1.809556] omap_gpio 481ae000.gpio: Could not set line 14 debounce to 200000 microseconds (-22)
[ 1.818393] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 1.823044] omap_hsmmc 48060000.mmc: GPIO lookup for consumer wp
[ 1.829075] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 1.835787] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@0/target-modul'
[ 1.849700] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp@44000000/interconnect@48000000/segment@0/target-module'
[ 1.863512] omap_hsmmc 48060000.mmc: using lookup tables for GPIO lookup
[ 1.870255] omap_hsmmc 48060000.mmc: No GPIO consumer wp found
[ 1.902869] omap_hsmmc 481d8000.mmc: GPIO lookup for consumer cd
[ 1.908977] omap_hsmmc 481d8000.mmc: using device tree for GPIO lookup
[ 1.915598] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@100000/target-'
[ 1.929944] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/ocp@44000000/interconnect@48000000/segment@100000/target-m'
[ 1.944194] omap_hsmmc 481d8000.mmc: using lookup tables for GPIO lookup
[ 1.950939] omap_hsmmc 481d8000.mmc: No GPIO consumer cd found
[ 1.956799] omap_hsmmc 481d8000.mmc: GPIO lookup for consumer wp
[ 1.962841] omap_hsmmc 481d8000.mmc: using device tree for GPIO lookup
[ 1.969406] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp@44000000/interconnect@48000000/segment@100000/target-'
[ 1.983742] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp@44000000/interconnect@48000000/segment@100000/target-m'
[ 1.997985] omap_hsmmc 481d8000.mmc: using lookup tables for GPIO lookup
[ 2.004726] omap_hsmmc 481d8000.mmc: No GPIO consumer wp found
[ 2.037033] omap_hsmmc 47810000.mmc: GPIO lookup for consumer cd
[ 2.043184] omap_hsmmc 47810000.mmc: using device tree for GPIO lookup
[ 2.049780] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/ocp@44000000/target-module@47810000/mmc@0[0]'
[ 2.061178] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/ocp@44000000/target-module@47810000/mmc@0[0]'
[ 2.072480] omap_hsmmc 47810000.mmc: using lookup tables for GPIO lookup
[ 2.079230] omap_hsmmc 47810000.mmc: No GPIO consumer cd found
[ 2.085146] omap_hsmmc 47810000.mmc: GPIO lookup for consumer wp
[ 2.091233] omap_hsmmc 47810000.mmc: using device tree for GPIO lookup
[ 2.097840] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp@44000000/target-module@47810000/mmc@0[0]'
[ 2.109253] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp@44000000/target-module@47810000/mmc@0[0]'
[ 2.120578] omap_hsmmc 47810000.mmc: using lookup tables for GPIO lookup
[ 2.127352] omap_hsmmc 47810000.mmc: No GPIO consumer wp found
[ 2.134521] sdhci-pltfm: SDHCI platform and OF driver helper
[ 2.141728] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.152307] NET: Registered protocol family 10
[ 2.157901] Segment Routing with IPv6
[ 2.161789] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 2.168419] NET: Registered protocol family 17
[ 2.173444] Key type dns_resolver registered
[ 2.177970] omap_voltage_late_init: Voltage driver support not added
[ 2.185104] Loading compiled-in X.509 certificates
[ 2.205473] mmc1: new high speed MMC card at address 0001
[ 2.214330] reg-fixed-voltage fixedregulator-mmcwl: GPIO lookup for consumer (null)
[ 2.222604] mmcblk1: mmc1:0001 IS004G 3.64 GiB
[ 2.227571] mmcblk1boot0: mmc1:0001 IS004G partition 1 2.00 MiB
[ 2.233615] reg-fixed-voltage fixedregulator-mmcwl: using device tree for GPIO lookup
[ 2.241896] mmcblk1boot1: mmc1:0001 IS004G partition 2 2.00 MiB
[ 2.248070] of_get_named_gpiod_flags: can't parse 'gpios' property of node '/fixedregulator-mmcwl[0]'
[ 2.257427] mmcblk1rpmb: mmc1:0001 IS004G partition 3 512 KiB, chardev (243:0)
[ 2.264741] of_get_named_gpiod_flags: parsed 'gpio' property of node '/fixedregulator-mmcwl[0]' - status (0)
[ 2.274688] gpio gpiochip1: Persistence not supported for GPIO 20
[ 2.287618] mmcblk1: p1 p2 p3 < p5 p6 p7 p8 p9 p10 >
[ 2.326320] omap_i2c 44e0b000.i2c: bus 0 rev0.12 at 100 kHz
[ 2.336806] omap_hsmmc 47810000.mmc: GPIO lookup for consumer cd
[ 2.342982] omap_hsmmc 47810000.mmc: using device tree for GPIO lookup
[ 2.349562] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/ocp@44000000/target-module@47810000/mmc@0[0]'
[ 2.360983] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/ocp@44000000/target-module@47810000/mmc@0[0]'
[ 2.372300] omap_hsmmc 47810000.mmc: using lookup tables for GPIO lookup
[ 2.379035] omap_hsmmc 47810000.mmc: No GPIO consumer cd found
[ 2.384912] omap_hsmmc 47810000.mmc: GPIO lookup for consumer wp
[ 2.390956] omap_hsmmc 47810000.mmc: using device tree for GPIO lookup
[ 2.397521] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp@44000000/target-module@47810000/mmc@0[0]'
[ 2.408894] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp@44000000/target-module@47810000/mmc@0[0]'
[ 2.420182] omap_hsmmc 47810000.mmc: using lookup tables for GPIO lookup
[ 2.426912] omap_hsmmc 47810000.mmc: No GPIO consumer wp found
[ 2.460745] hctosys: unable to open rtc device (rtc0)
[ 2.467783] ALSA device list:
[ 2.471172] No soundcards found.
[ 2.865507] EXT4-fs (mmcblk1p5): recovery complete
[ 2.871022] EXT4-fs (mmcblk1p5): mounted filesystem with ordered data mode. Opts: (null)
[ 2.879231] VFS: Mounted root (ext4 filesystem) on device 179:5.
[ 2.886319] devtmpfs: mounted
[ 2.891206] Freeing unused kernel memory: 1024K
[ 2.895952] Run /sbin/init as init process
INIT: version 2.98 booting
[ 3.130396] EXT4-fs (mmcblk1p5): re-mounted. Opts: (null)
[BOOT] Mounting /dev/mmcblk1p7 to /mnt/data
[ 3.167470] EXT4-fs (mmcblk1p7): mounted filesystem with ordered data mode. Opts: (null)
[BOOT] Mounting loopback fs
[BOOT] Setting cryptsetup
[BOOT] Mounting encrypted FS
Configuring network interfaces: ifdown: interface wlan0 not configured
done
Mounting loopback fs
Setting cryptsetup
Mounting encrypted FS
/sbin/ldconfig: /usr/lib/libstdc++.so.6.0.22-gdb.py is not an ELF file - it has the wrong magic bytes at the start.
gcs_hub_controller
udhcpc: started, v1.32.1
[ 4.355747] cpsw 4a100000.ethernet: initializing cpsw version 1.15 (0)
[ 4.388474] usbcore: registered new interface driver usbfs
[ 4.400243] usbcore: registered new interface driver hub
[ 4.405652] usbcore: registered new device driver usb
[ 4.420341] usbcore: registered new interface driver usb-storage
udhcpc: sending discover
INIT: Entering runlevel: 3
Setting hotplug handler: /etc/rc3.d/S00-config-hotplug: line 22: can't create /proc/sys/kernel/hotplug: nonexistent directory
[ OK ]
Creating device files: udhcpc: sending discover
udhcpc: sending discover
Auto-mount of [/media/mmcblk1p5] successful
Auto-mount of [/media/mmcblk1p8] successful
Auto-mount of [/media/mmcblk1p6] successful
Auto-mount of [/media/mmcblk1p2] successful
Auto-mount of [/media/mmcblk1p9] successful
[ OK ]
Starting the hotplug events dispatcher
Synthesizing the initial hotplug events
Waiting for /dev to be fully populated
fsck from util-linux 2.37.2
mount: mounting /dev/mmcblk1p9 on /mnt/update failed: No such file or directory
mount: mounting /dev/mmcblk1p7 on /mnt/container failed: No such file or directory
Setting timezone and system clock: hwclock: settimeofday: Invalid argument
[Fail]
Starting system logging.
Configuring network interfaces: ifdown: interface wlan0 not configured
Internet Systems Consortium DHCP Client V3.1-ESV-R3
Copyright 2004-2011 Internet Systems Consortium.
All rights reserved.
For info, please visit https://www.isc.org/software/dhcp/
ifconfig: SIOCSIFADDR: No such device
udhcpc: sending discover
Bind socket to interface: No such device
If you did not get this software from ftp.isc.org, please
get the latest from ftp.isc.org and install that before
requesting help.
If you did get this software from ftp.isc.org and have not
yet read the README, please read it before requesting help.
If you intend to request help from the dhcp-server@isc.org
mailing list, please read the section on the README about
submitting bug reports and requests for help.
Please do not under any circumstances send requests for
help directly to the authors of this software - please
send them to the appropriate mailing list as described in
the README file.
exiting.
failed
Starting hostapd: Configuration file: /etc/hostapd.conf
Could not read interface wlan0 flags: No such device
nl80211: Driver does not support authentication/association or connect commands
nl80211: deinit ifname=wlan0 disabled_11b_rates=0
Could not read interface wlan0 flags: No such device
nl80211 driver initialization failed.
wlan0: interface state UNINITIALIZED->DISABLED
wlan0: AP-DISABLED
wlan0: CTRL-EVENT-TERMINATING
hostapd_free_hapd_data: Interface wlan0 wasn't started
failed
Starting ntpd: [OK]
Starting wpa_supplicant: [FAIL]
--- No wireless interface found ---
Starting /usr/sbin/sshd: [ OK ]
Configuring network interfaces: ifdown: interface wlan0 not configured
done
Mounting loopback fs
Setting cryptsetup
Mounting encrypted FS
/sbin/ldconfig: /usr/lib/libstdc++.so.6.0.22-gdb.py is not an ELF file - it has the wrong magic bytes at the start.
udhcpc: started, v1.32.1
gcs_hub_controller
usb_storage 61440 0
usbcore 221184 3 xhci_plat_hcd,xhci_hcd,usb_storage
udhcpc: sending discover
Distribution built using LinuxLink by Timesys
Kernel 5.4.106-ts-armv7l for armv7l